Connecting you with tips, trends and news for all things connectivity

The IT Professional’s Guide to 8K Connectivity

8K blog header

From full HD 1080p to 4K to 8K, the world of display resolutions has seen some impressive advancements over the last 10 years. While people often discuss the resolution capabilities of display technologies, the focus is rarely on understanding how to enable these new resolutions. As you probably already know, it takes a lot more than simply plugging an old cable into a new display.

While the introduction of 8K technology might not be the latest news, the ‘implementation of 8K connectivity’ certainly is. With the help of this guide, IT professionals will learn the ins and outs of enabling and navigating the uncharted waters of 8K technology. We’ll cover:

So, without further ado, let’s jump in to discover how you can prepare to enable 8K technology across your workplace.

The Lead from 4K to 8K

The Leap From 4K

At first glance, 8K might seem like twice the resolution of 4K, but actually, it’s 4 times the pixels of its predecessor (4k).

To answer the question – when will 8K be standard?

Truth is, such a big leap in the resolution requires extensive development and all major players in the electronics industry are working towards developing the necessary chipsets and the supporting software to enable this technology. Considering the progress that has already been made, full implementation of 8k hardware doesn’t seem to be a distant dream anymore.


The industries and applications adopting 8K

Industries & Applications

Before we get into the technicalities of 8K, let’s quickly review some of the industries and applications that might be first to adopt 8K technology.

1) Medicine
MRI’s, CT scans, and ultrasounds can all benefit from higher resolutions, giving doctors an edge in early diagnosis.

2) Content Creation
Video editing and content development industries are also expected to upgrade to 8K. Editing software manufacturers will all be preparing for this transition as 8K content developers are expected to edit video that is shot with 8K resolution.

So, is 8K worth it? Absolutely.

Besides these applications, enhanced worker productivity is a key benefit across multiple industries. With 8K resolution, users can consolidate multiple monitors into a large single monitor that allows for enhanced visualization and thus increased productivity.


Enabling 8K with DisplayPort and HDMI 2.1

DisplayPort 1.4 and HDMI 2.1: The Keys to Enabling 8K

As an extension to VGA and DVI protocols, HDMI and DisplayPort are the latest serial interfaces capable of transmitting audio and video. According to the recent trends, the market has gravitated towards HDMI and DisplayPort interfaces as a predominant choice, with the older technology protocols being gradually phased out with every subsequent hardware update.

Now, with the latest introduction of DisplayPort 1.4 and HDMI 2.1 standards, video transmission has taken another leap towards making advanced resolutions like 8K a reality. The figure below provides a quick snapshot of the most critical updates to both standards that have helped enable higher resolutions. The implementation of DisplayPort 2.0 is not too far either. DisplayPort 2.0 can further boost the bandwidth capabilities that would allow for even higher resolutions up to 16K.

DisplayPort vs HDMI data capacity

Of course, there are a number of significant improvements within both standards, including progress in dynamic HDR and comparatively higher refresh rates, but the most notable advancement for enabling 8K is the breakthrough in achieving an extremely high bandwidth.

DisplayPort 1.4 enables a 50% increase in bandwidth compared to its predecessor (4K UHD). It raises data capacity from 5.4 Gbps to 8.1 Gbps per lane, increasing the total to 32.4 Gbps over four transmission lanes.

HDMI 2.1 more than doubles the bandwidth of the previous generation, providing an increase from 18.1 Gbps to 48 Gbps data rate.

These upgrades to DisplayPort and HDMI are critical to enabling the new world of 8K pixel clarity. A single full color 8K display at 30Hz requires 24.48 Gbps of data, while a single full color 8K display at 60HZ requires 49.65 Gbps of data.

Required bandwidth for 8K

It might also be useful for IT professionals to understand the use case behind DisplayPort 1.4 and HDMI 2.1 and how implementing either of these technologies can be beneficial according to the end goal.

  1. If the end goal is to connect multiple 8K computer monitors, then DisplayPort is best as it allows users to daisy chain up to four monitors whereas HDMI can drive a maximum of two at the same time.

  2. But if high definition audio is also a priority then HDMI standard offers a better solution as it uses audio return channels (ARC) to deliver high resolution audio, and therefore is a preferred choice for audio/video (A/V) applications.

The 8K Ecosystem and How to Implement an 8K Solution

The 8K Ecosystem: Implementing an 8K Connectivity Solution

To understand how to best implement an 8K solution, at least from a hardware configuration standpoint, it is essential to:

  1. Consider the current technological landscape

  2. Account for future hardware development that is currently underway

In an ideal world – considering DisplayPort 1.4 and HDMI 2.1 are both capable of handling the high throughputs required to enable 8K transmissions – users would be free to choose either interface. Unfortunately, that is not the case. Based on what’s currently available in the market, only 8K televisions are equipped with HDMI 2.1 connectors while most 8K monitors are only available with DisplayPort 1.4. This poses a unique set of challenges for IT professionals determining the appropriate hardware to implement an 8K solution.

The Current Landscape

To complicate the matter further, not only are there differences in available ports on 8K TVs and 8K resolution monitors, but also with host desktops and laptops. For this reason, and for the sake of simplicity, let’s evaluate various configurations for desktops and laptops separately.

Desktop connections

Theoretically, there are three options when connecting a desktop computer to an 8K display:

  1. The easiest and most convenient option is to connect your desktop to an 8K TV via a single HDMI 2.1 rated cable.

  2. The next best option would be to use a single DisplayPort 1.4 cable to connect your desktop to an 8K@30Hz monitor.

  3. Lastly, in order to connect your desktop to an 8K@60Hz monitor, you’ll need two separate DisplayPort 1.4 cables to drive the necessary bandwidth. In this case, both DisplayPort 1.4 cables needs to be plugged into the same monitor to allow for the increased bandwidth transmission required to enable 8K ultra HD with a 60Hz refresh rate.

For these setups to be functional, there are a few key variables that need to be accounted for:

  1. The desktop processor and graphics card (internal or external) should be capable of outputting a high enough bandwidth signal to support 8K.

  2. Both HDMI 2.1 and DisplayPort 1.4 cables should be certified to their respective standards. Any older standard certified cable will not be able to handle the required signal throughput.
Desktop hardware for 8K

Laptop connections

Laptops, due to space constraints, are generally considered to be slightly less dynamic in offering extreme functionality. Consequently, current laptops are not able to offer the dual DisplayPort 1.4 connections required to drive a single 8K@60Hz display (in native uncompressed signal form).

Nevertheless, with the current versions of available ThunderboltTM 3 laptops, driving a single 8K@30Hz display is realistically achievable. A simple setup to connect a Thunderbolt 3 laptop to an 8K@30Hz monitor can be seen in the diagram below. With this configuration, the DisplayPort 1.4 signal would pass through a Thunderbolt 3 cable into an 8K docking station, which would be connected to an 8K@30Hz monitor via a certified DisplayPort 1.4 cable. As an alternate configuration, an external DisplayPort 1.4 capable graphics card can also be utilized to achieve the same setup.

laptop hardware for 8K

Forecasting the Future of 8K

Forecasting the Future

Now that we understand the bandwidth and connectivity requirements to enable 8K, let’s take an early peek into the future and examine how improvements in connectivity hardware solutions can impact the 8K ecosystem.

Laptop connections

The entire premise of the future 8K ecosystem is dependent on the following factors:

  1. Wide availability of DisplayPort 1.4 compatible 8K docking stations (recently released)

  2. Availability of 8K docking stations that offer HDMI 2.1 ports

  3. Introduction of HDMI 2.1 on 8K monitors

  4. Future generations of laptops introducing hardware to convert the DisplayPort 1.4 signal into the HDMI 2.1 format

If these conditions are satisfied with next generation revisions, then a few possible configurations for an 8K setup can be envisioned.

  1. The DisplayPort 1.4 Docking Solution
    If the docking station is DisplayPort 1.4 compatible but not HDMI 2.1 compatible, then it can be connected with a single DisplayPort 1.4 cable (to DisplayPort monitors only).

  2. The HDMI 2.1 Docking Solution
    The next generation of 8K connectivity hardware is expected to be introduced with an HDMI 2.1 output port. Despite this, the native display output signal from a Thunderbolt 3 laptop is still likely to be in DisplayPort 1.4 form. Therefore, the signal will need to be converted over to HDMI form to be compatible with an HDMI 2.1 capable monitor. In this scenario, users will need an 8K docking station that supports the HDMI 2.1 protocol in order to pass the signal from their Thunderbolt 3 laptop to an 8K monitor that has an HDMI 2.1 port.

  3. The USB-C Adapters Solution
    As a third option, there will be a possibility to plug the 8K laptop into an 8K monitor directly via a USB-C to HDMI 2.1 or USB-C to DisplayPort 1.4 adapter. In this scenario, the adapter can convert the signal format to the desired output form. One thing to note in this setup, however, is that by foregoing the docking station in between, the user is losing all of the additional productivity and port consolidation options a dock can offer.

  4. The Built-in Conversion Solution
    If future laptops have built-in hardware to convert video signal from DisplayPort to HDMI, then it would allow for a direct connection via a high-quality HDMI 2.1 cable.
future hardware for 8K

Single vs Dual 8K Display

Single 8K Display vs Dual 8K Display: The Possibilities and Limitations

So far, we have explored various configurations to connect to a single 8K display. But what about dual 8K displays? Is it even possible given the current technology landscape?

The answer here is a bit more complicated. Let’s do a quick back of the napkin analysis of the bandwidth needed to drive a dual 8K@30Hz display. 8K@30Hz with RGB 8-bit full color requires a bandwidth of 24.48 Gbps.

To drive dual displays, a 48.96 Gbps data rate (2 x 24.48 Gbps) would be required when considering transmission in an uncompressed native signal format.

Enable single vs dual 8K display

Considering Thunderbolt 3 laptops, in a best-case scenario (i.e. not accounting for any technology adjusted overhead), can output a bandwidth of 40 Gbps, even at maximum bandwidth, their downstream transmission bandwidth falls short of the required 48.96 Gbps needed to drive dual 8K@30Hz displays. Similarly, a single 8K@60Hz is even more difficult to implement as required bandwidth at RGB full 8-bit color is 49.65 Gbps.

With a Thunderbolt 3 Laptop (max output 40 Gbps)

Thunderbolt 3 laptop single vs dual 8K display

So, with the bandwidth limitations of current laptops, is single 8K@60Hz or dual 8K@30Hz even possible?

Yes – it is possible.

Introducing Display Stream Compression (DSC). DSC protocol is a type of lossless compression that allows for the same cables to transmit considerably higher rates of data. However, this protocol is not widely adopted in the industry yet.

While it’s difficult to predict a definite timeline, we can certainly hope for DSC to become mainstream technology soon, thereby making it a standard offering amongst all 8K compatible hardware.


8K Checklist

Your 8K Checklist

Just in case you are considering updating your hardware connectivity equipment, we’ve compiled a few key points to keep in mind to future proof your solutions.

  1. Start with the basic accessory: Cables.
    It would be prudent to ensure that all new DisplayPort and HDMI cables are rated to DisplayPort 1.4 and HDMI 2.1 standards.

  2. Pay attention to the graphics cards.
    It would be best to pay extra attention while upgrading your host systems as well. Ensure that all your systems graphics cards are DisplayPort 1.4 compatible. The older DisplayPort 1.2 compatible graphics cards max out at supporting 4k graphics.

  3. Prepare your annual budgets for the upgrade.
    There might be a slight incremental cost now with DisplayPort 1.4 and HDMI 2.1 rated products, but it would be much more cost effective to future proof your solutions in the long run. As an added benefit, both these standards are reverse compatible with previous generations, so essentially you have nothing to lose.

Prepare Yourself for 8K with the Right Tools

It’s no secret that any new technology poses its own unique set of challenges and 8K is no different. Signal integrity complications associated with high resolution video transmissions are the reason it’s critical to choose a connectivity provider that can develop fully functional and compatible products. Ensure your products are certified, backed by reliable warranties, and that you work with a manufacturer who can provide the support you need when troubles or questions arise.

We hope you now feel a little more prepared and informed about the upcoming 8K revolution. Making connectivity easy for our customers is in our DNA and this time around with 8K will be no different.

StarTech.com is a leading technology and connectivity provider who is prepared to support you through your transition to the next generation of display technologies. For a full list of our 8K connectivity products visit our 8K Connectivity Accessories page and stay tuned for our upcoming 8K connectivity products including docking stations, display adapters, and cables.

9 Comments

  1. Oscar Maltez 1 year ago

    Hello,
    I need urgently the most powerful USB-C to HDMI Display port. Where can I purchase it? I’m attaching it to my IMAC 2017 to two other Samsung monitors. Please assist. Thank you

    • Danielle at StarTech.com 1 year ago

      Hi Oscar! You’ve come to the right place. StarTech.com offers USB-C to DisplayPort or HDMI adapters and cables. Here are the most powerful options for each:

      USB-C to DisplayPort:
      Adapter: CDP2DP146B
      Cable: CDP2DP142MBD

      USB-C to HDMI:
      Adapter: CDP2HD4K60H
      Cable: CDP2HD2MBNL

      As long as the video source supports DisplayPort alt mode, which I believe the 2017 iMac does, these would be the best options for adding a monitor with your inputs.

  2. Weston 1 year ago

    you need a DisplayPort to HDMI adapter. you can find it on Google:) the port you’re trying to fit an HDMI cable into is a Displayport,not HDMI.

  3. Murat Erkurt 6 months ago

    Great blog, thank you. Is there any point to point wireless solution that can link PC to 8k TV without need for physical cables? At 40+ Gbps probably not, I couldnt find it, may be you would know?

    • Danielle at StarTech.com 6 months ago

      Hi Murat! Unfortunately, at this time, no, there is not a wireless solution for 8k.

  4. Robert 3 months ago

    Under the heading “The Leap From 4K” you have this image with half circles mentioning resolutions.
    But the resolutions for 4K and 8K are both wrong : 4K => 3480 x 2160, and 8K => 7860 x 4320. These should be 4K => 3840 x 2160, and 8K => 7680 x 4320.

    • Danielle at StarTech.com 3 months ago

      Hi Robert! Thank you for bringing this error to our attention. We have updated the banner image with the correct resolutions.

  5. Ike Reed 3 months ago

    Hey so 8k 120hz tvs are out now so how do you connect to those without compression?
    If its not possible now what would I need to have when it becomes possible?
    Wouldn’t that be 100gb/s

    • Danielle at StarTech.com 3 months ago

      Hello! Most 8K TVs currently on the market will support 8K 60Hz or 4K 120Hz. To output 8K 120Hz with 8 Bit Color depth uncompressed, it would require 102.20 Gbit/s. HDMI 2.1 does support 8K at 120hz using Display Stream Compression and because Display Stream Compression is a lossless technology, there would be no image quality difference between an 8K 120Hz uncompressed vs 8K 120Hz compressed using Display Stream Compression. We hope this helps!

Leave a reply to Danielle at StarTech.com Click here to cancel the reply

Your email address will not be published. Required fields are marked *

*