Connecting you with tips, trends and news for all things connectivity

Windows 10 is Here: Here’s What You Need to Know

Windows10-MonitorImage-2 (2)

If you’re concerned about what effect Windows 10 might have on your IT environment and / or StarTech.com products, you will want to read our Q&A below. This is the largest update to Windows ever (it includes a free upgrade for users of Windows 7 and 8/8.1), and is expected to increase the rate of adoption in the enterprise sector – so the chances are, you’ll be affected one way or another. So read on and be prepared!

Q: Who will be getting Windows 10 and when?

A: The release will be staggered, meaning people who have reserved their downloads first will get it immediately, followed by others in waves, assuming there are no problems.  For IT managers, upgrades won’t happen on work PCs without you knowing about it because volume licences of Windows don’t qualify for the free upgrade, and the Get Windows 10 app won’t appear on any PC that’s joined to a domain.

Q: What are the major differences for Windows 10?

A: For users, most of the user interface differences will be subtle. Tiles are still there, but you can choose to do without them if you like. The best improvements will come for those who have new PCs enabled with retina scanning, which takes the hassle of logins away. Task View allows you to create multiple panes on a desktop and swipe easily back and forth, making a laptop screen act more like several large desktop monitors. Cortana is like Apple’s Siri, with a surprising list of things it can do via voice command alone.

For IT managers, there will be two main differences. First, Windows 10 users will get 10 years of support, including feature and security updates (while these updates will happen automatically for Windows Home users, Windows Pro and Enterprise users can control updates via Windows Update for Business). Secondly, Windows 10 uses peer-to-peer networking to download new updates, so traffic patterns in the office will be very different from previously, when each PC downloaded its own copy. If you have Software Assurance, the upgrade to Windows 10 is included. If you don’t have Software Assurance, you should consider it, as you won’t get automatic upgrades without it (just security patches), and the Windows 10 upgrade capabilities may prove less time-consuming than the current option of wiping and re-imaging systems.

Q: How can I tell my StarTech.com product is compatible with Windows 10?

A: To verify if your product has been updated to include Windows 10 support, go to StarTech.com, locate your product by entering the product SKU or name, and click on the “Technical Specifications” tab.

Tech-Spec-Tab

Tech-Spec-Tab-OS-Support

Q: My products web page does not list Windows 10 as a supported operating system. When will it?

A: As of August 17th, 2015 all StarTech.com products that have been updated to support Windows 10 have been updated online to reflect this. Any product not showing Windows 10 support on the Technical Specifications tab is not likely to be receive an update for Windows 10.

Q: Which versions of Windows 10 will be supported?

A: Any StarTech.com product that supports Windows 10 will work with Windows 10 Home, Pro and Enterprise, both 32 and 64 bit versions. If you’re a member of the Windows Insider Program (the beta release), your product may still work, however, those versions are not officially supported by StarTech.com. Windows 10 for mobile is also not supported. For further information, please contact our team of Technical Advisors.

Q: What is Windows Insider and how can I tell if I’m running this version of Windows 10?

A: Windows Insider is a preview release version of Windows 10. If you downloaded Windows 10 but are not sure what version you have, click the “Start” button or the “Cortana” search bar. Type “winver.exe” (minus the quotations). Select the “winver” Run command search result, which should be at the top. Any version with a number DIFFERENT than “Build 10240” is currently a “Windows Insider” or beta version of Windows 10 (as of August 2015). For example, if you’re build number is 10166 or 10525, these are Windows Insider builds.

If you have a Windows Insider version, your product may work, but isn’t officially supported by StarTech.com.

winverexe

Q: Are there products that I can expect to work in Windows 10, despite your website not listing support for Windows 10?

A: Any StarTech.com product that is considered operating system independent – meaning it does not require specific operating system drivers or software to function – will work with Windows 10, as well as previous versions Windows. Generally, products that are independent of the operating system can be identified by the below image on the product page.

OSI

Q: Screen Resolution is no longer an option when I right-click on my desktop.  How do I arrange multiple monitors with my USB video adapters?

A: Microsoft replaced “Screen Resolution” with “Display settings” with the release of Windows 10. Right clicking on the desktop and selecting Display settings will take you to the same application that Screen Resolution did in Windows 8/8.1. You can drag and drop your displays here to match their physical location in your work space. For further information on multiple displays in Windows read our FAQs on the topic found here, and here.

Display-settings

We hope you found this information beneficial and that your Windows 10 related questions have been answered. If you have any further questions please get in touch with our Technical Advisors by visiting our support contact page.

28 Comments

  1. Robin Ponting 4 years ago

    Really this is very helpful for reader.Thank You! for precious note.

  2. Why are we not getting any newer version of window after so long? We are just getting some updates but the entire OS is not getting updated. It would have been great if we could get a new OS.

    • Danielle Mayea 3 years ago

      Thanks for checking out our article! While Microsoft released an update to Windows 10 in April of 2018, we don’t have access to any information on updates beyond that as we aren’t officially affiliated with Microsoft. We suggest reaching out to Microsoft’s customer support team for more information on updates.

      • First, Windows 10 users will get 10 years of support, including feature and security updates (while these updates will happen automatically for Windows Home users, Windows Pro and Enterprise users can control updates via Windows Update for Business)

  3. brother support 3 years ago

    Windows 10 boots faster, work faster and seems much more robust than either Windows 7 or Windows 8/8.1. I haven’t had any problems with drivers or programs that run on Windows 8/8.1, although all of those old Metro apps are destined for the bit bucket.

  4. education 2 years ago

    Thanks for sharing lots of information about windows 10.

  5. Mind Mingles 2 years ago

    It’s a very interesting and knowledgeable post. Through this post, I learn many things. I appreciate your work and efforts. Thanks

  6. While still under a beta testing period with Windows Insiders, the following adaptation of Windows 10 presently affirmed as the May 2019 update—is drawing nearer to discharge. Despite the fact that not a huge update, there are a couple of changes that change the almost four-year-old working framework to make it fresher. These incorporate another light subject and changes to the pursuit experience, Cortana, and the sky is the limit from there. Here’s all that you have to know the latest update to Windows 10.

  7. WOW SO COOL

  8. Canon Error 801 2 years ago

    You are looking for the best operating system for your personal use, you may go for Windows 10 as most of the new system is made up of Windows 10. Windows 10 is quite advanced and updated with some more new features and functions compared to any older version of Windows.

  9. Service Printer 2 years ago

    this post is really very interesting and helpful,i learn many things in it,thanks for sharing the information about window 10 .

  10. nice post thanks for sharing

  11. Thanks for sharing this blog here. It seems really very informative.

  12. Windows 10 2 years ago

    After the Windows 10 up-gradation, there are so many questions in everyone’s mind. Some users think that their data will be lost, some think Microsoft will asked money after the up-gradation. Windows insider is a new thing in Windows 10 and. it is a developer setting from where a person can give some developing ideas to the developers.

  13. This is a really helpful post, very informative there is no doubt about it. Thanks for sharing this information with us. I really appreciate your work.

  14. Thanks for sharing the information, your writing skills are really impressive.Canon Maxify MB5470 Drivers

  15. Henry Rafal 12 months ago

    This is a really very informative article, there is no doubt about it. Thanks for sharing this article with us. This is very nice of you.

  16. Halley Roberts 12 months ago

    Great post! This is a really helpful article. Thank you for posting this article. If you have any issues related to Netgear router orange light then contact us. If you want to call us then visit our website for more information.

  17. garminsatnav 12 months ago

    The Garmin Satnav update should detect which maps update garmin satnav you have installed. It will also provide you with details garmin sat nav of which upgrades are available for your device. The latest plans (details) released by Garmin tend to have more information and additional Points of Interest within the file.

  18. John Matt 11 months ago

    Thanks for sharing this great informative article with us.

  19. Garmin Map updates 11 months ago

    Indeed, this article contains significantly more information on this subject. We’ve looked at all the data a few points are equally appropriate and others are usually outstanding.

  20. Pumpkin Seeds 11 months ago

    Thank you so much for this wonderful Post.

  21. magellan update 9 months ago

    The article you shared here is really helpful for every one, after i read this now i am able to know. So Thanks for sharing. This is really good.

  22. Thanks for sharing. This is a very good post and it was important to me. I’m glad I found this blog. Thanks for your help, I can advise you to add useful information to your situation.

  23. SBCglobal Sign In 8 months ago

    Thanks to the moderators for sharing this blog post.

  24. Johny Charles 8 months ago

    Thanks for providing recent updates regarding the concern, I look forward to read more.

  25. car reviews 7 months ago

    Very Good Blog..!!

  26. john nicholas 7 months ago

    I am intentionally looking for such a blog as I am facing an issue while using my desktop, today I learn something new from this post. Looking towards for how to connect a printer on windows 10.

Leave a reply to Windows 10 Click here to cancel the reply

Your email address will not be published. Required fields are marked *

*